From Discovery to Partnership
Hallberg is the owner and CEO of the Swedish mechanical engineering company Comeco. What he is demonstrating here is what is usually done directly at construction sites: Before the steel bars can be used to form meshes or reinforcing cages, they have to be bent into the right shape, this can vary from construction project to construction project. Precise bending is therefore mostly carried out by construction workers on mobile stirrup bending machines that are operated manually – as manufactured by Comeco.
Comeco is a small company based in the Swedish town of Enköping near Stockholm and Uppsala. In 1991, the machine manufacturer started with manufacturing radiant heaters for the construction industry, cutting and bending machines for rebars were added to the to the portfolio in 2009. The main customers are construction machinery rental companies, which account for 80 percent of the business. That makes it clear: Ideally, the machines should be compact, easy to transport and simple to operate for the different users – characteristics that Hallberg wanted to improve on his hydraulic machines.
“Around 2015, we wanted to further develop our machines to make them more service-oriented, safe and quieter”, he explains. “Back then, we coincidentally came across one of our older machines which had a name plate from NORD on the drive.” The contact to the system supplier for drive solutions was established and Hallberg decided to replace the hydraulics in the next Comeco machine with an electronic drive system from NORD. After the first bending machine for rebars with a diameter of 16 mm was successfully introduced, Comeco also developed machines for 20 and 25 mm rebars. More recently, the machine for 32 mm rebars was developed and launched, this was being presented by Hallberg.