News –

“For us, drives are more than just their power.”

They made NORD DRIVESYSTEMS a system provider: Since the 1980s, frequency inverters have been an integral part of the modular products offered by the specialist for drive solutions from Bargteheide. NORD’s drive electronics portfolio meets the requirements of numerous industry applications and always stays close to the market with its developments.

Bargteheide, 2025-10-21

During the design of a drive system, NORD takes more into account than just motion. “For us, drives are more than just their power”, says Jörg Niermann, Head of Marketing. “We develop drive solutions that are precisely tailored to applications and associated customer requirements.” For this, the company maintains a wide range of modular products.

NORDAC frequency inverters: Compatible and multi-functional

Since the mid-1980s. centralised and decentralised drive electronics supplement the manufacturer’s motors and gear units to create complete solutions. The frequency inverters are characterised by high compatibility with all system designs and integrated functions:

  • NORDAC PRO is the control cabinet inverter with multi-protocol Ethernet interface and multi-encoder interface.
  • NORDAC LINK for installation close to the motor provides full plug-in capability, therefore facilitating the installation and maintenance.
  • NORDAC FLEX is installed directly on the motor and has a modular structure as well as scalable functions.
  • NORDAC ON for motor mounting controls the high-efficiency motors from NORD and provides easy commissioning thanks to its multi-protocol Ethernet interface.

Further developments announced

In a next step, the NORDAC ON will feature new safety functions so that it can be integrated in Ethernet environments. Furthermore, the NORDAC ON PURE will be offered for the wash-down area – with food-safe NXD  tupH® surface treatment, a smooth housing design and a reduced number of plugs.

Find out more .